Metro TRK .sis for P910 UIQ device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Metro TRK .sis for P910 UIQ device

6,011 Views
venkat2006
Contributor I
Hi,
Can anyone help me in getting, respective Metro TRK for P910. I searched a lot of discussion forums, documents, pdfs, updated with Codewarrior patches, but didn't find the ready TRK .sis file. I have Codewarrior OEM 3.1. I downloaded the source for TRK with the package name as "MetroTrk_v1.10", but without a .pkg file. It has dlls, app and the exe. Atleast can anyone help me out building the package and install it on the phone. I am not understanding why is it so difficult to get a TRK .sis file. Everywhere least help and documentations sad. As am trying with an evaluation version of Codewarrier, immediate help will be very much helpful for me. So that if successfull can go for a full version of Codewarrior.

Thanks & Regards,
venkat2006
Labels (1)
0 Kudos
Reply
2 Replies

1,703 Views
CrasyCat
Specialist III
Hello
 
This looks like a CodeWarrior for Symbian related question.
To get answer to that question I would recommend you to use the Nokia forum.
 
 
CrasyCat
0 Kudos
Reply

1,703 Views
venkat2006
Contributor I
Hi CrasyCat,

I have gone through, Nokia forum, Freescale forum, NewLC forum and have posted same problem everywhere. But I didn't get any information until now. Thanks for u r help. Have gone through Sony ericsson and Symbian website too, but got least help from there. There are just views on my posted problem everywhere but no solution yet.

Thank U
venkat2006

Message Edited by venkat2006 on 2006-08-18 02:03 AM

0 Kudos
Reply