Memory space occupy percentage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Memory space occupy percentage

2,766件の閲覧回数
KeydalaPanca
Contributor I

CW 56800/E Hybrid controller version 7.3

 

I need to know how many space my program and my program runtime variables uses in my freescale DSP 56F8367 memory.
And how mnuch space miss to full the DSP 56F8367 memory.

 

How can I do ?
Is there any tool that can I use to know these information ?

 

I need to evaluate it soon, so please come with solutions!

 

regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,882件の閲覧回数
J2MEJediMaster
Specialist I

Have you taken a look at the map file generated by the linker? That usually gives you the sizes of various parts of the program.

 

---Tom

0 件の賞賛
返信

1,882件の閲覧回数
KeydalaPanca
Contributor I

Yes, I think you mean this:

 

  0000F020 0000F020 00000000 .x_Peripherals
  00040000 00040000 00000004 .p_Interruptsboot
  00000000 00000000 000000AC .p_Interrupts
  000000AC 000000AC 00009DFB .p_Code
  00004264 00000001 00001E6F .x_Data
  00004000 00004000 00000264 .x_internal_ROM
  0004F800 0004F800 00000800 .p_internal_RAM

 

can you explain me the means of each row, please, and say me how much free space I have ?

(DSP56F8367)

 

Thanks!

0 件の賞賛
返信

1,882件の閲覧回数
J2MEJediMaster
Specialist I

You left off (or the linker left off) the most relevant part of the map file output:

 

 v_addr   p_addr   size     name
  00000000 00000000 000000A4 .p_interrupts_flash_ROM
  000000A4 000000A4 000004FE .p_flash_ROM
  000005A2 00000001 0000008D .p_flash_ROM_data
  00020000 00020000 0000008B .p_boot_flash_ROM
  0002F800 0002F800 00000800 .p_internal_RAM
  00000001 00000001 000006B5 .x_internal_RAM

 

The third column has the size of the particular element. You can check those values against a datasheet for the part. You may want to experiment with the linker settings to adjust the map file output; More information on linker and output settings can be found in the Targeting Manual. It is located in the Help folder in the CodeWarrior installation folder.

 

---Tom

0 件の賞賛
返信

1,882件の閲覧回数
KeydalaPanca
Contributor I

Hi Tom,

 

you're right, the linker left off that part of map file output
I red the Targeting Manual, but I didn't undertsannd how to modify the linker setting in order to get the most relevant part of the map file output.

Can you please tell me how can I do?

thanks

0 件の賞賛
返信