MCP5645S issue : code warrior debug window not appearing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCP5645S issue : code warrior debug window not appearing

5,414 Views
Dinesh_Guleria
NXP Employee
NXP Employee

Hello NXP team,

 

I am working on MCP5645S & using Codewarrior & using Multilink Universal FX.
I am using windows-10 &  following version of Code Warrior :--

 

________________________________________________________________________
Release Notes 
CodeWarrior Development Studio for MPC55xx/MPC56xx 
Version 2.10
________________________________________________________________________

 


I have installed patch as suggested on PE micro forum :--
http://www.pemicro.com/SRS/view_reply_SR.cfm?issue_id=30609


I am facing a problem when i try to connect debug, debugger use to start, flashing occurs. Please see the attached images.

But once this task to burn code is done, immediately all the Debug windows disappear, I am not able to the Debugger window. Because of this I am not able to debug the Project.


Please suggest how to resolve this issue ?

Regards,
Dinesh

 

0 Kudos
Reply
1 Reply

3,818 Views
stanish
NXP Employee
NXP Employee

Hello,

Have you solved this issue? 

I noticed that the debugger seems to be initialized correctly, and the execution stays at entry point as expected.

Alternatively, you can try to connect to a programmed device using  Pemicro debugger only.

You can run it from "C:\Freescale\CW for MPC55xx and MPC56xx 2.10\pemicro\CW_ICDPPCNEXUS.EXE"

Stan

0 Kudos
Reply