MC56F8006Demo Stuck

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8006Demo Stuck

3,365件の閲覧回数
davefs
Contributor I

My MC56F8006DEMO is having problems.  When I connect it to power several of the LEDs come on, then all of them turn off except LED4, which just blinks.  When I connect my USB TAP to it then the "Run/Pause" LED comes on and stays on.  If I try and burn something to it via the USB TAP I get an error that says "CSS Protocol Plugin: Unknown Protocol Error".  Did I somehow brick my MC56F8006DEMO?  Is there a way to get it going again.  The code on the board right now shouldn't be causing any LEDs to blink.

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,837件の閲覧回数
Heron
Contributor II

I also have same problem "CSS Protocol Plugging: Unknown Protocol Error" when using MC56F8006DEMO kit either with parallel port  JTAG or USB TAP adapters, but problem does not appear when I use MC56F8013DEMO kit:

This lead me to think the problem is something related to MC56F8006DEMO kit or MCU, but I can't find some app note about this issue.

¿What should I do to put this demo kit to work properly again?

 

 

0 件の賞賛
返信

1,837件の閲覧回数
J2MEJediMaster
Specialist I

So the tools work with one board and not the other? Please file a service request on that. Click here to do that.

 

---Tom

0 件の賞賛
返信

1,837件の閲覧回数
Heron
Contributor II

Dear Tom,

 

SR Number:  1-614214891

0 件の賞賛
返信

1,837件の閲覧回数
davefs
Contributor I

Figured it out, I enabled "Wait for device to power up at connect".  When I program the board it pauses while it's waiting for power up then I'll unplug my board then plug it back in and it is able to program the board.  After that though, when I'm running the LED example it stops on the T1_Interrupt every time (there's no breakpoint there).  If I hit reset the program runs normally.  Still looking into it . . .

0 件の賞賛
返信