Jungo WinDriver in the Device Manager

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jungo WinDriver in the Device Manager

7,659件の閲覧回数
Alex_56k
Contributor I

Software:

CodeWarrior Development Studio for S12(X) Special Edition V5.1

 

OS: Windows 7 SP1, Windows XP SP3

 

Problem:

After installing CodeWarrior there is some mysterious Jungo WinDirver in my Device Manager. This is very annoying and I wanted to remove it from there. But after trying to Modify the installation I got Internal Error 2753. dpinst32.exe

 

Now I can't do nothing at all, not even uninstall the CodeWarrior, I get the same dpinst32.exe error and installer exits. So what is this Jungo garbage and how do you get rid of it? Reinstall Windows? Way to go Freescale :smileylol:

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,915件の閲覧回数
kef
Specialist I

Jungo WinDriver is required for P&E Multilink.

0 件の賞賛
返信

3,915件の閲覧回数
FridgeFreezer
Senior Contributor I

It's the driver for P&E USB devices, although of course it doesn't SAY that anywhere and it's not really mentioned.

0 件の賞賛
返信

3,915件の閲覧回数
RLH
Contributor I

I'm in the same problem with the Codewarrior S12(X) Internal Error 2753.  dpinst32.exe.  I can't finish the installation and I can't remove or uninstall (a misnomer for sure) Codewarrior and I'm stuck.

 

Any suggestions on what I should do next other than nuking my machine and starting my project with a micro that doesn't require Codewarrior?

0 件の賞賛
返信

3,915件の閲覧回数
J2MEJediMaster
Specialist I

The only possible solution might be to download and install the P&E Micro drivers, which CodeWarrior uses to communicate with the Multilink. That might put the Jungo driver back in place and let the installer to proceed.They can be downloaded from here, from the P&EMicro downloads page.

 

---Tom

0 件の賞賛
返信