How do I resolve File Error 206002. Duplicate File?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I resolve File Error 206002. Duplicate File?

2,254件の閲覧回数
russfarrell
Contributor I

Working in CW IDE version 5.9, Windows 10 Pro machine:

Installed Products:
CodeWarrior Development Studio for Freescale HC12 v5.1 HCS12 G64 Service Pack, build 110727.
CodeWarrior Development Studio for the S12(X) Version 5.1, build 10221.
CodeWarrior Development Studio for Freescale HCS12(x) v5.1, PE V3.05 Service Pack, build 130715.

Everything was fine last week, now when I start or close CW I get the following error (image attached):

File Error 206002.

Duplicate File.

All formatting and preferences were reset (I am able to update and change)

0 件の賞賛
返信
1 返信

2,012件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I never had this problem.

But CW5.1 doesn't support windows 10. If you work with HCS12G, please use CW5.2 instead.

CodeWarrior® Dev Tools for HCS12(X) MCUs|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信