How can I flash my application?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I flash my application?

1,130 次查看
UB39
Contributor I

Hello!

 

I write my application and tested it inside internal RAM. Now I wanna flash it to use it as a stand alone application.

 

Therefore I changed the debug configuration from MK60N512VMD100_INTERNAL_RAM to MK60N512VMD100_INTERNAL_FLASH, but it has no effect.

With the internal Flash configuration I can debug my program as before. But after a reset or after power up my application doesn t run.

 

Using the flash might be more complicated than I expect.

So what must I do to get my program into flash?

 

I also try to use the simple flash programmer that is part of Codewarrior, but I alway get error messages when I try to use it.

 

I use the TWR K60 Tower and CodeWarrior 10.1

 

May Thanks

 

Ulf

标签 (1)
0 项奖励
回复
1 回复

993 次查看
J2MEJediMaster
Specialist I

Please do not cross post your question into other forums. I have answered it elswhere.

 

---Tom

0 项奖励
回复