Hi All,   I am developing an application using Processor...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi All,   I am developing an application using Processor...

2,444件の閲覧回数
Bharath
Contributor I
Hi All,
 
I am developing an application using Processor Expert. I am planning to use SPI to send and receive characters.
 
While choosing a bean for SPI communication i found two beans "Init_SPI" and "SW_SPI". When i looked into both of the beans thorughly I found out that "Init_SP"I bean initializes SPI and requires you to implement the interrupt handler, where as "SW_SPI" bean provides "Send_Char"/"Recv_Char" menthods to send/receive.
 
Do i need to use both of the beans or just use "SW_SPI" bean?
 
Thanks in advance
 
Regards,
Bharath
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,366件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
There are some examples using SPI and SWSPI on the installation.
Please refer to the folder:
  \Stationery\Processor_Expert_Examples\DemoApplications\HWBeans
 
Hope this will help you
Regards
Pascal
0 件の賞賛
返信