GNU Configure Problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GNU Configure Problems

2,973件の閲覧回数
glowkeeper
Contributor I
Hi,
 
I'm having a problem using the MetroWerks CodeWarrior command line compiler under cygwin when trying to build an open source package for the Wii using gnu's configure, make, make install scenario.
 
Basically, no matter what options I give, when I run configure, I get this far: 
 
configure: error: C preprocessor "mwcceppc.exe" fails sanity check
I realise this is a long shot, but has anyone ever come across this before? If so, could you shed some light on the problem?
 
Glowy
 
ps.  mwcceppc.exe -version    
Metrowerks C/C++ Compiler for Embedded PowerPC.
Copyright (c) 2006, Freescale Semiconductor, Inc.
All rights reserved.
Version 4.1 build 60831
Runtime Built: Aug 31 2006 18:18:06
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,403件の閲覧回数
LeoAtreides
Contributor I
Hi there,
 
 
  I have had similar problems trying to get software packages to ./configure . Did you figure out how to do this, and if so can you let me know how this is done
 
regards
 
Leo
0 件の賞賛
返信

1,403件の閲覧回数
J2MEJediMaster
Specialist I
"Fails sanity check" is a new one on me. Nor does it sound healthy.

I'd recommend that you submit a service request on that. Click here to file a service request.

---Tom

0 件の賞賛
返信