Flash_over_JTAG on a 56F8345

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash_over_JTAG on a 56F8345

3,794件の閲覧回数
steel_tig
Contributor I

Hi,

I want to know if someone had success with the flash_over_jtag application?

I’m using flash_over_jtag_v2.exe and 568346_flash.cfg that came when I installed CodeWarrior 7.1 and updated at 7.2.

I don’t have the flash config file for the 568345 but the 568346 is the closest I have.

When flash_over_jtag is executed, the mass erase perform well. But I get a CRC on flash #0 (program flash) after it’s programmed.

Can someone give me a hint on this one?

Regards

Steel

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,103件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hello,
 
You've problem with the Flash_over_jtag tool.
See details about the Flash on the web link:
Not sure that a there is a cfg file for the 8345.
 
On the installation there is another tool named Fflash.
This is working twith USBTap and will replace the Flash_over_jtag.
Please have a look to the installation folder:
  \M56800x Support\56800E flash programmer
 
The last patch for the DSP 7.x is the V7.3.
You can download it:
 
The fflash tool will use the cfg file of the folder: 
  \M56800E Support\initialization
For details about the tool please refer to the Flash programmer users guide.doc manual in the \M56800x Support\56800E flash programmer\docs.
 
Be aware that the DSC 8.0 is available.
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272694011187
The Special edition license is installed by default.
If you need another version of the license please contact your local distributor.
You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.

The DSC 8.1 is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B

Pascal

 
0 件の賞賛
返信