Filling unused Flash locations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Filling unused Flash locations

2,329件の閲覧回数
conte
Contributor I
How can I fill the unused flash locations with a certain value ?

Thank you.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,023件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
I can propose you to use the Fill Memory feature:
You can fill the memory with a value (0x11 for instance) before to load the application.
 
What is the process ?
- on the ide click on debug | Connect via the debug menu,
- the debugger will be launched,
- go to Debug | DSP56800E | Fill Memory
For details, please refer to the Targeting_56800E.pdf manual.
 
Regards
Pascal
0 件の賞賛
返信