Download CodeWarrior IDE version 5.7.1844

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download CodeWarrior IDE version 5.7.1844

Jump to solution
3,077 Views
silvanobattisti
Contributor I

Dear all,

Could I download an old legacy CodeWarrior IDE ?

I've a very old project on MCF8252.
I losed the IDE (Freescale CodeWarrior IDE version 5.7.1844) used to build the project.
Is there any possibility to download it again?

Thanks
Silvano

Labels (1)
Tags (1)
1 Solution
2,523 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Silvano,

In addition to Pascal response, once you know the CodeWarrior version that was being used you can find the download link on the below page, it contains the CodeWarrior legacy downloads:

CodeWarrior Legacy Downloads|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

View solution in original post

3 Replies
2,524 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Silvano,

In addition to Pascal response, once you know the CodeWarrior version that was being used you can find the download link on the below page, it contains the CodeWarrior legacy downloads:

CodeWarrior Legacy Downloads|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

2,523 Views
silvanobattisti
Contributor I

It is a MFC V6.2.
The CW 6.2 from the suggested URL  works fine: I get the same build output (regardles of compile date time obviously).

Thanks to all !!!!!
The sun is shining again :smileyhappy:

Best Regards
Silvano

2,523 Views
trytohelp
NXP Employee
NXP Employee

Dear Silvano,

The IDE Version  5.7.1844 is not the tool version but the version of the IDE.

The IDE is a feature as the compiler , linker or debugger included in a Codewarrior development tool.

I've several old versions installed on my PC.

The CW for MCF V6.3 was released in Q2 2006.

This version used the IDE version 5.7.0 Build 2015.

It seems you're using an older version.

We need to know exactly the tool version you're using.

  Under CodeWarrior IDE (classic)

                Start the IDE and click on Help | About Freescale CodeWarrior.

                Click on Installed Products

                Provide us all info displayed.

                Or you can save them in a txt file.

If the Installed Products is not available for older version you should find information in the welcome.txt

under the installation folder.

It's probably an older version as MCF V6.0, V6.1 or V6.2.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------