Difference between Coldfire and Freescale Stationery Wizards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between Coldfire and Freescale Stationery Wizards

Jump to solution
742 Views
AlexF3062
Contributor I

My environment is CodeWarrior for ColdFire Architectures v. 7.2, M52259EBV board.

Creating new project, I see the following items:

ColdFire New Project Wizard

FreeScale MQX 3.7 Stationery.

 

For now, I am able to create my projects using the second item. What is the difference between these Wizards, do I need ColdFire Wizard or it is OK to work with the Stationery?

Labels (1)
0 Kudos
Reply
1 Solution
506 Views
CrasyCat
Specialist III

Hello

 

Freescale MQX 3.7 Stationery allows you to create a frame for a project where you can use MQX.

If you decide to go with the New Project Wizard, this will create a frame for a project that does not use MQX.

 

So the big question here is do you intend to develop an application using MQX system kernel?

 

Catherine

View solution in original post

0 Kudos
Reply
2 Replies
507 Views
CrasyCat
Specialist III

Hello

 

Freescale MQX 3.7 Stationery allows you to create a frame for a project where you can use MQX.

If you decide to go with the New Project Wizard, this will create a frame for a project that does not use MQX.

 

So the big question here is do you intend to develop an application using MQX system kernel?

 

Catherine

0 Kudos
Reply
506 Views
AlexF3062
Contributor I

Thanks. I am quite happy with MQX at this stage, so I will continue to work with Freescale Stationery Wizard.

0 Kudos
Reply