Debug MCF5485 with P&E USB Coldfire Multilink in CodeWarrior 11.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug MCF5485 with P&E USB Coldfire Multilink in CodeWarrior 11.0

1,873件の閲覧回数
luizpietta
Contributor I

I can't debug my project in Codewarrior 11.0. After press debug button in Codewarrior 11.0 this error appears:

Starting 3rd party flash programming...
ERR: Warning: Programming algorithm not found for this device.

In this version of Codewarrior is possible to select a Alternative Algorithm, but I don't know what file select. In the possible choices there's not a MCF5485 ".cfp" file.

Note: When I debug the same project with CodeWarrior 10.3 no problems occurs.

Has anyone had this problem?

Best regards!

2 返答(返信)

1,685件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Luiz Pietta

Unfortunately there is a bug reported in codewarrior that cannot work with MCF5480. My recommendation for you is to use CodeWarrior 10.3 where there is not problem.

Codewarrior 10.6 / MCF5480 - Debugger complains of bad arguments 

Best Regards

Jorge Alcala

1,685件の閲覧回数
luizpietta
Contributor I

Thanks by the answer Jorge. I will remain using the CodeWarrior 10.3 to debug my project.

Best Regards,

Luiz Pietta

0 件の賞賛
返信