DSP56F8367 - adc driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP56F8367 - adc driver

2,307件の閲覧回数
nerella
Contributor I
hi,
I am trying to write a code for reading a voltage siganl  from a potentiometer.
how to read that data through the adc.i am using dsp56f8367 evaluation board. my voltage pot range is 0-2.6v max.
i need a code to read the adc data.please any one can help me in this regard.
thanks in advance.
 
nerella.


 --
Alban Edit: FSL Part Number must figure in Message Subject line.


Message Edited by Alban on 2007-07-25 01:29 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,000件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
There are lot of example of code on the installation.
Please refer to the folder \Stationery\Processor_Expert_Examples.
 
Hope you will find an example you can use.
 
Pascal
0 件の賞賛
返信