DATE and TIME in Codewarrior 7.2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DATE and TIME in Codewarrior 7.2.2

3,296件の閲覧回数
vier_kuifjes
Senior Contributor I

I know about __DATE__ and __TIME__ in Codewarrior, but is there an easy way to have the numeric values of date and time available at compile time? I am particularly interested in the year number...

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,004件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

I don't understand your question. can you be more specific?

what means "have the numeric values of date and time available at compile time"?

0 件の賞賛
返信

3,004件の閲覧回数
kef2
Senior Contributor V

I think Marc is interested not in strings like "Jan 16 2014" defined by __DATE__ standard C preprocessor macro, but about numeric value for date, or year, month and day.
These could help when someone has lack of ROM to include __DATE__ string parsing and reformatting routines. For example compile date coded as a number or converted to more compact string could be easily send over CAN in single CAN message. Unfortunately standard C has only __DATE__ and __TIME__ strings in fixed format.

3,004件の閲覧回数
vier_kuifjes
Senior Contributor I

That's indeed what I'm looking for. I need the number of the year at compile time to do some calculations with (also at compile time). At this moment I just enter the value in a #define which is no big deal as I only need to change it once a year.:smileyhappy:

0 件の賞賛
返信

3,004件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

thank you Edward.

yes, CW doesn't have exact feature as Marc request.

please summit it as a SR as feature request to [email protected]

we will process.

0 件の賞賛
返信

3,004件の閲覧回数
kef2
Senior Contributor V

Since it is not standard feature and other compiler vendors aren't going to add it even in the far future, I think Marc should try setting project to launch some external tool at pre build step to generate *.h file with date formatted as required.

When compiler IDE has no pre-build command setting, for generating only date *.h file, formtting tool can be launched from OS scheduler every day.

0 件の賞賛
返信