Command Line Interface to build project files(source files, header files and linker command file)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Command Line Interface to build project files(source files, header files and linker command file)

1,394件の閲覧回数
cyh
Contributor II

Hi, the CW(Power Architecture v8.8.3, CPU=P2020) was installed on my desktop a few months ago.

I used to use the IDE to compile the project.

 

But due to growing team size, building project files at command line interface would be good for our project.

 

May someone provide me some guideline/documentation to allow me to make/nmake project files at DOS command line interface?

ラベル(1)
0 件の賞賛
返信
1 返信

1,004件の閲覧回数
J2MEJediMaster
Specialist I

Check out the Power Architecture Build Tools Reference (Power Arch Build Tools Reference.pdf), located in the Help folder of the CodeWarrior installation directory. It has a lot of information on how to use the command-line arguments with the tools.

 

---Tom

 

0 件の賞賛
返信