Codewarrior for Windows updates

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior for Windows updates

2,014 Views
skdhf
Contributor I

I'm looking for "Codewarrior for Windows" updates (7.x, 8.x, 9.x) . I was expecting to find these in the support section of this web site (like I did a few months ago but I didn't download them) but apparently they're missing. Were they pulled out? Are they still downloadable somewhere (I need them)?

 

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,427 Views
J2MEJediMaster
Specialist I

If you are talking about the CodeWarrior for Windows where you write Windows applications, those tools are no longer supported. No updates are available.

 

---Tom

0 Kudos
Reply

1,427 Views
skdhf
Contributor I

That's right, I'm talking about the Codewarrior IDE to write windows applications (i think it's called Codewarrior Pro). I remember updates for it were available on your site not so long ago.

I know this product has been discontinued and so has been Codewarrior for Mac OS however updates are still available for the latter (in the support section.

 

Why isn't it the same for Codewarrior for windows????

 

I need those updates (from 7.1, 7.2, 7.3, 8.x, 9.x)

 

Thanks

0 Kudos
Reply