Codewarrior 2.7 MPC5554 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 2.7 MPC5554 problem

2,762件の閲覧回数
khurram712
Contributor I

Can anyone tell what this error means and how to remove it

 

"Link Error: Relocation of the symbol is out of range"

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,966件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi khurram712,

 

I'd suggest you to see this thread:

 

https://community.freescale.com/message/71562#71562

 

 

Stanish

0 件の賞賛
返信

1,966件の閲覧回数
khurram712
Contributor I

thanks alot

0 件の賞賛
返信

1,966件の閲覧回数
khurram712
Contributor I

Thanks for providing the solution but i came across another problem

first the pragma preprocessor could nt be added to function definition(it couldn't remove error)

so i added it to function declaration as a trial..it did work.The linking

error was removed.However during debugging the sequence of execution

doesnt follow these particular function's call( i .e the functions with pragma preprocessor) .

Instead it starts executing main.asm.i have wriiten nothing useful in main.asm and

i have n't invoked it in my code either.Even then it moves there which is making trace of bug

 in program more difficult.

 

i would like to ask one more thing...can pragma preprocessor be used with assembly functions?

 

Regards

Khurram Hameed

0 件の賞賛
返信

1,966件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi khurram712,

 

Yes you are right,  pragma should be used in combination with function prototype declaration.

I can debug the RAM code without any limitations/confusions.

See below the example how to place standalone assembler function into RAM:

 

main.c

---------


#pragma push
#pragma section code_type ".my_RAM_code" ".my_RAM_code" data_mode=far_abs code_mode=far_abs
void my_C_ram_func(void);  
extern void my_asm_ram_func(void);
#pragma pop

 

void my_C_ram_func(void)
{
  asm (nop);
}

 

int main(void) {
 
my_C_ram_func();
  my_asm_ram_func();
  ...

}

 

main_asm.s

----------

.globl my_asm_ram_func

.section .my_RAM_code,text

my_asm_ram_func:
nop
nop

blr


*.lcf

-----

...

SECTIONS
{
  ...
    GROUP : {
       .__uninitialized_intc_handlertable ALIGN(0x10) : {}
       .data   : {}
       .sdata  : {}
       .sbss   : {}
       .sdata2 : {}
       .sbss2  : {}
       .bss    : {}
       .my_RAM_code: {}
    } > internal_ram
}

 

Stanish

0 件の賞賛
返信