CodeWarrior license Dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior license Dongle

1,138 Views
Runcom
Contributor I

I have a license dongle that the red light is blinking all the time and LMTOOLS can't obtain FLEXID.

Other dongle, the red light is on and works fine. Is the dongle broken or there is a way to save it?

Labels (1)
0 Kudos
Reply
1 Reply

973 Views
J2MEJediMaster
Specialist I

It sounds like that dongle is broken or old enough that the latest drivers do not recognize it. See this web page for more information on the USB dongles.

 

Note: The USB dongle is not supported on 64-bit Windows 7. However, from your description, if one of the dongles is working, then you are not running that OS version. Just wanted to make sure that you knew.

 

---Tom

0 Kudos
Reply