CodeWarrior V10 V7.2 and V6.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior V10 V7.2 and V6.2

1,307件の閲覧回数
TeeTwo
Contributor I

I would like to use one IDE across three different ColdFire CPU MCF51CN, MCF5225, and MCF5441x. I can install and get V6.2 to work with the 51CN examples. I am having no luck using V10 to work with the 51CN. Is it possible to use CW V10 to work across all of these platform? If so what are some of the common mistakes folks make when trying to use V10 with a 51CN?

 

Thanks in advance for your reply

ラベル(1)
0 件の賞賛
返信
1 返信

882件の閲覧回数
CrasyCat
Specialist III

Hello

 

CodeWarrior MCU V10 should support all Coldfire MCUs.

 

Which kind of trouble are you facing?

Are you unable to build, to debug, ...?

 

Did you try creating a new project for MCF51CN128. Can you build and debug it?

 

CrasyCat

 

0 件の賞賛
返信