CodeWarrior IDE version 5.7.0 Build 1932 - Please help me!!!! A bug really strange.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior IDE version 5.7.0 Build 1932 - Please help me!!!! A bug really strange.

4,182件の閲覧回数
NeoSP
Contributor I
Dear friends,

I've been working in a new project with CodeWarrior IDE (version 5.7.0 Build 1932) and in the last week, the my CodeWarrior IDE is not working properly. The problem is occurring when: Every time when I click on the OPEN command, IMPORT PROJECT command, OPEN WORKSPACE command, ADD FILES command and every command that open a "Windows Explorer" window, the CodeWarrior IDE close automatically.

Does anybody could help me?!!! Or does anybody have any idea to solve that?!!!

Thanks,

Best regards,
Marco.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,000件の閲覧回数
NeoSP
Contributor I
Dear Friends,

Thanks for the tips. Yeah, I installed the Office 2007 recently. CrasyCat, I did what you say and now the Codewarrior is working very well.

Thanks,

Best regards for all,
Marco.
0 件の賞賛
返信

2,000件の閲覧回数
bigmac
Specialist III
Hello Marco,
 
Have a look at this thread -
and see if your problem is similar.
 
Regards,
Mac
 
0 件の賞賛
返信

2,000件の閲覧回数
CrasyCat
Specialist III
Hello
 
Did you install Office 2007 in the mean time?
There seems to be an issue with CodeWarrior standard open/save dialog after Office 2007 has been installed.
 
n order to cure that you need to change the properties of the IDE.exe.

Right click on IDE.EXE (in window explorer), select Properties, then go to Compatibility tab.
Uncheck "Run this program in compatibility mode for".
After this modification it should work correctly.
 
CrasyCat
0 件の賞賛
返信