CodeWarrior 6.3 Installation Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 6.3 Installation Error

1,650 Views
Kwok
Contributor I

Hi,

I am trying to install CW 6.3 in my computer that is running in Vista.

 

During the installation, an error occur:

 

Error 1305:

It asks me to find a dll file called "ics08dll_ics08grz_v130.dll" and make sure I can access it.

 

However, this file in my folder is actually 0kB, so I cannot access it.

 

Does anyone know how to solve this problem? Where can I get this file?

 

Thank you so much

 

Kwok

Labels (1)
0 Kudos
Reply
1 Reply

1,216 Views
CrasyCat
Specialist III

Hello

 

Did you check the VISTA limitation in Welcome_CW_MCUs.txt?

 

WINDOWS VISTA SPECIFIC LIMITATIONS:
-----------------------------------

The following limitations are applicable only if you are installing the product on Windows Vista:

(1) During installation, security messages may pop up concerning drivers being installed. It is highly
    recommended to click on the option "continue anyway..", so the drivers can be installed.

(2) When opening the Codewarrior components (IDE, Debugger etc.) Firewall warnings may appear
    with the option to block or unblock the application. It is advisable to click on the unblock option to
    continue.

(3) For more VISTA specific limitations after the installation, please refer to:
         "{INSTALLATION DIRECTORY}\Release_Notes\HC08\Notes_CW_MCUs_V6 3_Vista.txt"


GENERAL LIMITATIONS:
--------------------

The following limitations are applicable to Windows Vista, Windows XP:

(1) It is highly recommended to have at least 400 MB of free space on the Windows system disk.
(2) Product supports 32-bit versions of Windows XP, Windows Vista.
 

CrasyCat

0 Kudos
Reply