CodeWarrior 10.1 Install New Software error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 10.1 Install New Software error

5,852件の閲覧回数
lowks
Contributor III

Hi there,

 

I am trying to update the compiler in the CodeWarrior 10.1 SE version on Windows XP. However, I keep getting the below error when installing new software under HELP. Can anyone advise?

 

An error occurred while collecting items to be installed session context was:smileysad:profile=PlatformProfile, phase=org.eclipse.equinox.internal.provisional.p2.

engine.phases.Collect, operand=, action=). No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.gcc.toolchain,1.0.2.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.gcc.toolchain.nl1,1.0.2.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.toolchain,1.0.15.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.coldfire.cdt.toolchain.nl1,1.0.15.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.hc08.cdt.toolchain,1.0.17.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.hc08.cdt.toolchain.nl1,1.0.17.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu,1.0.4.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.cdt.toolchain,1.0.1.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.changewizard,1.0.44.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.changewizard.nl1,1.0.44.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.elfimporter,10.1.5.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.elfimporter.nl1,10.1.5.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.license,10.1.0.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.license.nl1,10.1.0.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.linuxapp.projectwizard,1.1.8.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.linuxapp.projectwizard.nl1,1.1.8.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.nl1,1.0.4.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.pathmapping,1.0.5.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.projectWizard.nl1,1.3.46.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.projectimporter,1.1.5.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.projectimporter.nl1,1.1.5.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.projectwizard,1.3.46.FSL_b02057 No repository found containing: osgi.bundle,com.freescale.mcu.ui,1.0.0.FSL_b02057 No repository found containing: org.eclipse.update.feature,com.freescale.mcu,10.1.3

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

4,950件の閲覧回数
jhmrd
Contributor III

I had the same problem, and after a phone call, they sent me this PDF file which helped me get it to work. Reloading the software was a waste of time, as was downloading the patch directly and trying to use help-install software. It seems there is an error in the URL they provide for the update. I clicked on and added a '/' at the end of their URL and it worked, after several hours of cursing.

0 件の賞賛
返信

4,950件の閲覧回数
buckeyeman
Contributor III
Yes, this document is right, I am presently in the midst of an online update for CW MCU 10.1.
0 件の賞賛
返信

4,950件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

4,950件の閲覧回数
DerekTsou
Contributor I

If I un-installed CW10.1 then re-installed it, I think all of patchs and updates should be installed again, since I got error message while building file.

However, I can not re-install patchs successfully, CW10.1 reported that it was installed. I got feedback message as following:

 "Cannot complete the request.  See the error log for details.
"MCU v10.1 Compiler Update (ColdFire, Kinetis, Qorivva)" will be ignored because it is already installed."

 

My question is how to re-insall it agian?

0 件の賞賛
返信

4,950件の閲覧回数
DerekTsou
Contributor I

I found the way to un-install CW10.1 with all patches & updates.

Please delete the folders "c:\Users\Your user Name\.codewarrior" & "c:\Users\Your user Name\.eclipse" after un-install CW10.1

Now I can re-install CW10.1 with all of patches successfuly. 

0 件の賞賛
返信

4,950件の閲覧回数
CarlFST60L
Senior Contributor II

Thanks jhmrd this worked for me.

 

Follow the PDF and it WILL fix it!!

 

0 件の賞賛
返信

4,950件の閲覧回数
aarontc
Contributor I

i also have the same problem,anybody can tell me how to fix this?

0 件の賞賛
返信

4,950件の閲覧回数
J2MEJediMaster
Specialist I

Currently, to update the CodeWarrior tools you have to download an installer from the Freescale CodeWarrior web page and run it. You cannot update it through the Help choice in Eclipse.

 

---Tom

0 件の賞賛
返信

4,950件の閲覧回数
aarontc
Contributor I

i think that error generated by some thing wrong in the register....

after restore the windows 7 for the computer, everything works fine.

I had that error because i uninstalled everything and reinstalled them....

 

0 件の賞賛
返信