Cannot start debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot start debug

1,797 Views
Teckna
Contributor V

Hi everyone,

 

From few days, the very first time in the morning (after I start the PC) that I start to debug my project, I can work well. But every subsequent debug process (after a modification in the source code and the recompilation) can't work. At the end of the download process I get the message "Debug Initialization Warning. Unable to activate exception handling".

I tried to restart the debugger, unplug and plug the power source to the board, with no success. I think that only the PC restart can be useful (the afternoon I stop the PC and then I start it again the morning after).

 

I use CW 10.2, MQX 3.8 and a custom board based on K60N512.

 

I have no idea on how to correct the problem.

 

Many thanks

Teckna

Labels (1)
0 Kudos
Reply
3 Replies

1,646 Views
Teckna
Contributor V

Just a new information

 

Yesterday afternoon I've not stopped my PC (but I've closed CW), this morning I've made some changes in sources, compiled and debugged with no problem. Then I've made some other changes in sources, compiled, but I've got the error.

 

I don't know how to correct the error.

 

Many thanks

Teckna

0 Kudos
Reply

1,646 Views
J2MEJediMaster
Specialist I

This is where you need a second opinion, because the problem could be rooted in the PC, the emulator pod, or the board. Can you try a different board and emulator? Can you try a different PC?

 

---Tom

0 Kudos
Reply

1,646 Views
Teckna
Contributor V
Now my holidays are starting...

I will try on august 6th

Many thanks
Teckna
0 Kudos
Reply