Can Code Warrior load a flash memory (AM29LV160D-B) attached to a MPC860EN?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Code Warrior load a flash memory (AM29LV160D-B) attached to a MPC860EN?

2,217 次查看
richard_worth
Contributor I

If yes, File format needed and cable (interface)?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,117 次查看
richard_worth
Contributor I

I'm just looking to read, write, and verify flash content. I do not need any design or simulation features. Do I need the full code Warrior 8.8 or is there a subset/demo version available?

0 项奖励
回复

2,117 次查看
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 for the MPC860.

https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=6121541

 

This CodeWarrior supports code loading, debugging and Flash programming using CodeWarrior USB TAP:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

 

This CodeWarrior USB TAP provides connection to the MPC860 using BDM port of the MPC860.

 

Use Flash programmer from CodeWarrior 8.8 for load code to the AM29LV160D-B flash memory.

Flash programmer from CodeWarrior 8.8 supports .elf, binary and S-records files.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复