CW7.3 + Parallel JTAG + 8013 DEMO Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW7.3 + Parallel JTAG + 8013 DEMO Board

3,393 Views
Spongeman
Contributor I
Dear all
I'm triying to setup for the boards DEMO56F8013, the JTAG interface AXM-0337 and the CW7.3 using the bdlc_hall_pesl.mcp project.
After installation and first start I got the message from the Windows system tray: CodeWarrior: "parallel port open failed (invalid port number?)" Seems to come from the Parallel Port Init program in the startup folder.
When try to start the debugger I get the message: CCSProtocolPlugin: "Unknown protocol error" and "CCS connect refused"
Could you guys give me some advice?
 
COMPLAIN:
See too many the same questions on the forums, why CW didn't improve them?
Why CW didn't found the root cause and release some document?
Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,171 Views
TDog
Contributor I
Hi,

I got the same error with the same DEMO56F8013 board. Turns out my paralell port was faulty. I changed to another computer - no more error.
Perhaps you could check the paralell port settings in the BIOS?

Cheers.http://forums.freescale.com/post?board.id=CWDSPCOMM&message.reply_to_id=311#" rel="nofollow" target=...
0 Kudos
Reply