CW10 debug problem with windows VISTA, not in W-XP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10 debug problem with windows VISTA, not in W-XP

1,617件の閲覧回数
cocheca
Contributor I

Hi,

I have two problem in windows VISTA with CW10.

 

1.- When CW10 starts  this message appear in the console:

"...

ORB could not be initialized. Aborting connection.

java.net.ConnectException: Connection timed out: connect.

 

Anyone knows this problem ?

 

2.- When I try to debug a project, in 87% of the process, appear a windows error. It says:

"Could not set PC to entry point"

 

These problems don't happen in W-XP. I test the CW10 with the same project and same configuration.

Would appreciate any help.

Thanks. Regards Jose

ラベル(1)
0 件の賞賛
返信
1 返信

1,163件の閲覧回数
cocheca
Contributor I

Sorry, I forgot to mention my target.

 

It's TWR-51CN

s/n 309301203.

SCH-26003 REV E

700-26003 REV B

 

The OSBDM firmware was upgraded to the version comming in the CW10 directory.

 

Thanks in advance.

 

Jose.-

0 件の賞賛
返信