CW10 New Source Folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10 New Source Folder

ソリューションへジャンプ
2,163件の閲覧回数
WHookway
Contributor III

Hi,

I am unable to add a New Source Folder to my project, a regular folder, no problem.  I either get an error stating the Root name must be entered or Invalid Project path: Duplicate path entries, even when I browse.  It does not matter what I type as the folder name.  Also, could you point me to the documentation that describes the features and/or privileges that a source folder has over a regular folder as it related to the project.

Thanks,

Will

ラベル(1)
0 件の賞賛
返信
1 解決策
1,400件の閲覧回数
WHookway
Contributor III

Hi,

Update, the inability to add a New Source Folder problem was as the error indicated a "duplicate path exists".  However, the problem is that the project built successfully (no errors) and the duplicate path existed in the setup for Path and Symbols/Includes.  I do not know how the duplicate entry was creatded.  In this case the error can be duplicated by explicitly specifying a path such as c:/CW10/workspace/myProject/Sources and ${ProjDirPath}/Sources.  It does not matter if the duplicates are in the same languages folder or not, in my case they were not.

Regards,

Will

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,401件の閲覧回数
WHookway
Contributor III

Hi,

Update, the inability to add a New Source Folder problem was as the error indicated a "duplicate path exists".  However, the problem is that the project built successfully (no errors) and the duplicate path existed in the setup for Path and Symbols/Includes.  I do not know how the duplicate entry was creatded.  In this case the error can be duplicated by explicitly specifying a path such as c:/CW10/workspace/myProject/Sources and ${ProjDirPath}/Sources.  It does not matter if the duplicates are in the same languages folder or not, in my case they were not.

Regards,

Will

 

0 件の賞賛
返信
1,400件の閲覧回数
J2MEJediMaster
Specialist I

Please file a service request so this problem can be looked into. Click here to do that.

0 件の賞賛
返信