CW10.1 + Multilink = SLOW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.1 + Multilink = SLOW

1,458 Views
CarlFST60L
Senior Contributor II

Hi,

 

I have been using CW7.2 with my Multilink for development for a couple of years with no problem, I am now using CW10.1 for micro's to develop for Coldfire V2 (MCF52259 + FSLMQX).

 

CW10.1 is far to slow for development, when I hit debug it is literally minutes to download a medium size app, and the debugger is erratic and unusable, it just randomly stops on things and drops off while my code is still running, then it crashes every few hours, but my app runs 100%. I have also noticed that when you go into the debugger settings and change it to only download the executable etc on first time only, it makes NO DIFFERENCE (this worked great on CW7.2).

Labels (1)
0 Kudos
Reply
2 Replies

1,194 Views
CarlFST60L
Senior Contributor II

1 Minute 40 is the magic time, its about 20 seconds in CW7.2.

 

During debugging of code, I might download every 10 minutes, so, best case, 10% of my time is spend waiting for this... Gives me plenty of time to complain on the forums about CW10.1 : )

0 Kudos
Reply

1,194 Views
BlackNight
NXP Employee
NXP Employee

Hello,

there is a similar thread in

https://community.freescale.com/message/93180#93180

which has some solutions and hints how to improve the performance.

 

BK

0 Kudos
Reply