CW for Palm IDE settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW for Palm IDE settings

2,538件の閲覧回数
bazza
Contributor I
Hello,
 
I just lost the ability to bring up typedef definitions in the popup menu on Code Warrior in my current project, with all functions now in black instead of the default blue.
 
I must have accidently tripped some setting but for the life of me I cannot locate anything referring to getting this setting back. I have compared the project settings with other projects and nothing seems to fix the problem and no reference in any manuals.
 
Any help much appreciated.
ラベル(1)
0 件の賞賛
返信
1 返信

1,360件の閲覧回数
bazza
Contributor I
Sorry, I just found the setting under Project settings, Build Extras.
 
A bit strange though. I already had 'Compiler' selected which was identical to other projects but when I changed it to 'Language Parser' all the functions lit up. Besides Build Extras would suggest something to do with building the application rather than a setting for the IDE.
 
Oh Well....Back to sleep.
0 件の賞賛
返信