CW & async baud set

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW & async baud set

2,494 Views
bob_s
Contributor III
I've configured an async serial port with a CW bean.  I selected the baud rates I want to be able to select, but the bean does not enable the routine to change the baud rate.  Please see the attachment pics.  Thanks.
Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,133 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
To investigate the problem, it will be better to log it directly in the Technical support system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
 
Please provide us more details about the Tool version used.
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.
 
Can you please provide us your example reproducing the issue ?
 
Pascal
0 Kudos
Reply

1,133 Views
bob_s
Contributor III
Hi Pascal;

Thanks for the response.  What I found was that the routine was enabled, it was just  grayed out because it wasn't a routine that could be optionally excluded.   I thought that because it was grayed out, it couldn't be used.  No problem exists at this point. :smileyhappy:
0 Kudos
Reply