CW USB TAP: Driver for Windows 10 64-bit System

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW USB TAP: Driver for Windows 10 64-bit System

3,843 Views
evanespina
Contributor I

I have installed on my "new" laptop the 56800E Flash Programmer but I get the error "USB open failure" when I try to program the DSP.  The USB TAP device worked the last time I used it, albeit some years ago on an old laptop.  So I'm thinking that the problem now is related to the device driver as the installer I used is also an old one.  Can anyone advise where I can find a link to the latest drivers?  Thanks.

Tags (1)
0 Kudos
Reply
1 Reply

3,062 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Frankly speaking, I use Win7 OS now, I never use Win 10 os, so I can not say the usbtap is okay or not on win 10 os.

Anyway, I copy the usbtap drivers from CodeWarrior for MCU ver 10.7, pls try to install it.

BR

Xiangjun rong

0 Kudos
Reply