CW 4.6 and Windows 7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 4.6 and Windows 7

2,622件の閲覧回数
robertp
Contributor II

Based on my reading, I know I can't run CW in Windows 7 x64, but what about the 32 bit version of Windows 7, will CW 4.6 run in this environment?  I know the P&E drivers for debugging are certified for Windows 7 x32 AND x64

ラベル(1)
0 件の賞賛
返信
1 返信

1,074件の閲覧回数
kef
Specialist I

If you have access to installed CW files. I mean Program Files\... folders CW is installed to, then you can try Natep solution from here.

 

https://community.freescale.com/thread/57404

 

Don't know how on 32bits Win7, but on 64bits Win7 CW 5.0 installer just exits and you can't install it properly. Natep solution seems to work with CW5.0. With new unit12_z.DLL (see page 4 of that thread) I was able to debug using P&E USB Multilink.

 

It would be nice if Freescale made installer working on 64bits Win7. Even without P&E target, users still could use CW to just compile code, or even to debug in simulator mode.

0 件の賞賛
返信