7.3 download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

7.3 download

4,072 次查看
mchabot
Contributor I
This is a simple question and I'm sorry for bothering the community with it but ever since the metroworks website went away I can't seem to find the Codewarrior for DSP56F800e version 7.3 upgrade. I need the download because the codewarrior updater isn't working. Can someone please post a link?

Thanks,
M
标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,765 次查看
CrasyCat
Specialist III

Hello

Go to following URL
    http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882

Then click on 56800-E-DSC-UPDATES  

I hope this helps.

CrasyCat

0 项奖励
回复

1,765 次查看
Egal
Contributor I
Hi,

I have also tried to download the update to v7.3.

I have to fill out a form. When it`s done, I always get the following error message (last two weeks):

Unexpected Error

An unexpected error has occurred. This system may be temporarily unavailable due to technical difficulties. Please go back and try your request again.
If the problem persists, contact our Technical Helpline via phone:
Americas: 1-800-521-6274
Asia: +852-2666-8307
Japan: 0120-191-014
Europe: +49-89-92103-559
Or you can contact us by email at [email protected]

Exception Type: Freescale eBusiness Exception (major: 90000 minor: 0 details: UpdateProfileEJBAction.createContact(). Errors in creating contact: Critical System Error).
Date: Mon Jul 03 00:45:25 MST 2006


I think after two weeks the error should be corrected.

tnx
0 项奖励
回复

1,765 次查看
CrasyCat
Specialist III

Hello

Can you please contact the helpline or support as stated in the message.

CrasyCat

0 项奖励
回复