56f8347 - problems programming prozessor with jtag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56f8347 - problems programming prozessor with jtag

2,274件の閲覧回数
Kai
Contributor I
Hello,
 
I want to programm the processor with codewarrior by jtag. When the download bar
appears, nothing happens. After some seconds a error message appears: can't erase flash.
I checked the signals from the Jtag interface, the core is responding. Do i have to adjust something in the CPU inspector?
 
Thank you and excuse my english
 
Michael
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,037件の閲覧回数
jag
Contributor IV
Hi,

check that the speed of the jtag is between 800 and 1000 kHz.

Bye Jack
0 件の賞賛
返信