56F8367 JTAG Programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

56F8367 JTAG Programming

2,651 次查看
fef
Contributor I
I am receiving the error "Failed to write to flash" when using CW8.0 to program a 56F8367 device via the JTAG port.  It works fine using identical hardware and an older 8357 device.  I have verified all the JTAG signals at the processor, and it seems to be communicating since it starts the download process.  Are there any changes to the new devices that require addressing for programming? 

Fred F

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,045 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
Are you using the right flash programming file 56836x_flash.cfg ?
Can you try to create a project with the wizard (File | New) for this processor ?
By this way the project created will have all default settings to flash an application.
 
Pascal
0 项奖励
回复