56F8013 - Help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56F8013 - Help

2,181件の閲覧回数
duck
Contributor I
Hi:
 
I'm using 56F8013 cpu for a project,  i use beans to generate the code, and write some extra code on my own, and then compile it, I got the following error message:
 
Link Error: Undefined : "FArchIO"
Referenced from "FINT_PWM_Reload in INT_PWM_Reload.c"
 
Since i use PWM reload interrupt to do the ADC sampling and control method, so there must be something wrong with INT_PWM_Reload.c, but so far can't figure it out, need help!
 
Thanks!


--
Alban Edit: Please always include FSL Part Number in Message Subject line.



Message Edited by Alban on 2007-09-07 02:39 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,033件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
This is not easy to determine the cause of the problem.
The better way will be to log it directly in the Technical support system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
Please provide us more details about the Tool version used.
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.
 
Can you please provide us your example reproducing the issue ?
 
Pascal
 
0 件の賞賛
返信