56900/E CW V7.2 - Register Details window error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

56900/E CW V7.2 - Register Details window error

2,698 次查看
JimmyMood
Contributor I
I get the following error when trying to load and .xml template for the register details window
 
Code:
"Error importing XML file "FC.xml" near line 11Found tag "XMLPATH", which is invalid in this context"

 
I have no idea what is causing this, but not having the register details available makes debugging much more difficult.  Any ideas as to what is causing this?
 
Thanks
 
-Jim
 
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,257 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
I performed some tests on my side and I reproduced the problem.
I will contact our development team.
Can you please log it in our tracking system (Freescale CRM) via the web ?
 
Pascal
Freescale - CodeWarrior Support
0 项奖励
回复

1,257 次查看
dynapb
Contributor IV
Hi,
 
I am wondering if there is anything happening with this problem, is there a solution?
 
I am using 56800/E CW V7.3 for the 56F807.
 
I was trying to open various peripheral registers, like TMRA.xml, and get the same error message.
It almost looks like all the .xml files for the registers within the TMRA.xml are missing.
Is that the case?
Are they available somewhere or would it work to make them myself (assuming I knew how)?
 
Thanks,
 
Pete
0 项奖励
回复