servomotor hitec hs 311

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

servomotor hitec hs 311

1,171 次查看
millerarnoldber
Contributor I

por favor necesito unos ejemplos de control de servo con el jm60, que se mueva de 0 grados a 90 espere un tiempo y se devuelva a 0.

 

 

---------------------------------

 

 

please I need some examples of servo control with jm60, moving from 0 to 90 degrees, waits for some time and returns to 0.

 

Message was edited by: Monica Arvizu

标签 (1)
0 项奖励
回复
1 回复

1,034 次查看
trytohelp
NXP Employee
NXP Employee

Hello,

Please can you provide us more details regarding your problem ?

We need to know exactly what is the tool version you're using.

To do that you must:

  Under CodeWarrior IDE (classic)

      Start the IDE and click on Help | About Freescale CodeWarrior.

      Click on Installed Products 

      Provide us all info displayed.

      Or you can save them in a txt file.

  Under Eclipse IDE

    1-      Start Eclipse and click on Help ¦ Freescale Licenses

      The Status column gives the status of the license.

      Under Product, select it and click on details.

      A new dialog show up giving license details.

      Provide us all info displayed

    2-      Start Eclipse and click on Help ¦ About CodeWarrior Development Studio

      Under Installed Products, you will see the version used.

If the Installed Products is not available for older version you should find information in the welcome.txt

under the installation folder.

what is the processor and interface used ?

regards

Pascal

0 项奖励
回复