question about 'loss of lock' and 'loss of clock'

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

question about 'loss of lock' and 'loss of clock'

跳至解决方案
1,591 次查看
bluehacker
Contributor III

hi everyone

 

 

I read MC9S08AC16 datasheet, the chapter about ICG module  says there are two kind of errors called 'loss of lock' and 'loss of clock'.

then, what is the difference between loss of lock and loss of clock?

hope your explanations, thanks 

标签 (1)
0 项奖励
回复
1 解答
867 次查看
bigmac
Specialist III

Hello,

 

The two error states are sensed in different ways.  The loss of clock error is determined by whether the reference clock signal (internal or external) meets some basic timing criteria.  It will mostly be of value when using an external reference.

 

The loss of lock error is determined by whether the output of the DCO (part of the FLL) instantaneously meets a frequency accuracy requirement, relative to the reference frequency.  Obviously, a loss of clock condition will also result in loss of lock whenever the FLL is used.

 

A loss of clock detection and reset is of most interest when operating in one of the FLL bypassed modes.

 

Regards,

Mac

在原帖中查看解决方案

0 项奖励
回复
1 回复
868 次查看
bigmac
Specialist III

Hello,

 

The two error states are sensed in different ways.  The loss of clock error is determined by whether the reference clock signal (internal or external) meets some basic timing criteria.  It will mostly be of value when using an external reference.

 

The loss of lock error is determined by whether the output of the DCO (part of the FLL) instantaneously meets a frequency accuracy requirement, relative to the reference frequency.  Obviously, a loss of clock condition will also result in loss of lock whenever the FLL is used.

 

A loss of clock detection and reset is of most interest when operating in one of the FLL bypassed modes.

 

Regards,

Mac

0 项奖励
回复