question about 'loss of lock' and 'loss of clock'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about 'loss of lock' and 'loss of clock'

Jump to solution
2,268 Views
bluehacker
Contributor III

hi everyone

 

 

I read MC9S08AC16 datasheet, the chapter about ICG module  says there are two kind of errors called 'loss of lock' and 'loss of clock'.

then, what is the difference between loss of lock and loss of clock?

hope your explanations, thanks 

Labels (1)
0 Kudos
Reply
1 Solution
1,544 Views
bigmac
Specialist III

Hello,

 

The two error states are sensed in different ways.  The loss of clock error is determined by whether the reference clock signal (internal or external) meets some basic timing criteria.  It will mostly be of value when using an external reference.

 

The loss of lock error is determined by whether the output of the DCO (part of the FLL) instantaneously meets a frequency accuracy requirement, relative to the reference frequency.  Obviously, a loss of clock condition will also result in loss of lock whenever the FLL is used.

 

A loss of clock detection and reset is of most interest when operating in one of the FLL bypassed modes.

 

Regards,

Mac

View solution in original post

0 Kudos
Reply
1 Reply
1,545 Views
bigmac
Specialist III

Hello,

 

The two error states are sensed in different ways.  The loss of clock error is determined by whether the reference clock signal (internal or external) meets some basic timing criteria.  It will mostly be of value when using an external reference.

 

The loss of lock error is determined by whether the output of the DCO (part of the FLL) instantaneously meets a frequency accuracy requirement, relative to the reference frequency.  Obviously, a loss of clock condition will also result in loss of lock whenever the FLL is used.

 

A loss of clock detection and reset is of most interest when operating in one of the FLL bypassed modes.

 

Regards,

Mac

0 Kudos
Reply