pullup on MISO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pullup on MISO

1,629件の閲覧回数
IlConte
Contributor IV

Dear all, I have S08PT16

I use the SPI module configured as a master.

The SPI module can be not present and i need to use the same software.

My question is: the MISO (PTB4) have tge pull-up ?

Can i configure the PORT_PTBPE at 1 if is enabled the SPI module ?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,350件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Stefano

If you configure the Pin as input you can set the pullup enable, but if you configure the pin as SPI (MISO in this case) the internal pullup are disable

I hope this will help you.


Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信