pullup on MISO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pullup on MISO

1,690 Views
IlConte
Contributor IV

Dear all, I have S08PT16

I use the SPI module configured as a master.

The SPI module can be not present and i need to use the same software.

My question is: the MISO (PTB4) have tge pull-up ?

Can i configure the PORT_PTBPE at 1 if is enabled the SPI module ?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,411 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Stefano

If you configure the Pin as input you can set the pullup enable, but if you configure the pin as SPI (MISO in this case) the internal pullup are disable

I hope this will help you.


Have a great day,
Vicente

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply