pls. advice on the programmer kit for MC9S08QE128 .  we are developing BPM, using freescale design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pls. advice on the programmer kit for MC9S08QE128 .  we are developing BPM, using freescale design

1,036件の閲覧回数
jagannathang
Contributor II

can anybody advice us the program tools, and setup kits for programming and copying programs to MCU.  PLS. ADVICE PART NO and also the availability

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

908件の閲覧回数
tonyp
Senior Contributor II

P&E Micro's Cyclone PRO​  is a great solution for quick programming (if you plan to do a lot of units fast).  Stand-alone programming, i.e., no PC connection required!

A much cheaper (but also slower for larger volume production) solution is the various USBDM

0 件の賞賛
返信

908件の閲覧回数
jagannathang
Contributor II

Dear Mr. Tony,

thanks. can u pls. help me with the specs of the VAlve, and the Motor , specified in the block diagram of BPM machine.

regads

jagan

9845497950

G.Jagannathan

MANAGING DIRECTOR

AARMS Value Chain Pvt. Ltd.,

#211 D, I Floor, Temple Street,

9th Main Road, BEML III Stage,

Rajarajeshwari Nagar,

Bangalore- 560098

mob : 9845497950

www.aarmsvaluechain.com

0 件の賞賛
返信