i2c help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i2c help

2,555 Views
vic68
Contributor I
Hello, I'm trying to interface an i2c device, I need to send it 5 and 18 bytes successively,  I'm using the i2c example in the HCS08QRUGSW file.
Someone have some example ? or please tell me where I need to write the bytes that I need to send.
regards.
vic68 
Labels (1)
0 Kudos
Reply
1 Reply

1,372 Views
B_Conf
Contributor I
Hello vic68:
There are an Application note AN3291, it probably can help you!, but if it doesn´t, please search I2C and AP64 in forums, and you find some examples.
I´m trying to work with I2C and uC AP32 and I also have to send severals bytes to a EEPROM. but it doesn´t work yet.

Regards
Pablo (B_Conf) :smileywink:
0 Kudos
Reply