help help mc68hc908mr32cfu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help help mc68hc908mr32cfu

2,587 Views
k14011978
Contributor I
thank you for reading
sir we need to develop the onlineups using mc68hc908 uC based if anybody having the freescale based UPS control card with program kindly help us and give the related  information .
thanking you
my mail id [email protected]   and   no:04442660381
Labels (1)
0 Kudos
Reply
1 Reply

1,273 Views
alex_spotw
Contributor III
Hi:

I suggest looking into the Hybrid DSP-MCU processors from Freescale: MC56F83xx
The following link is to a UPS Reference Design

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RD56F8300OUPS&parentCode=56F8147&node...


Check also the Application Note AN3113

It has a full description of the UPS circuit and software implementation.

IMHO, you might have a hard time trying to implement an complete Online UPS with a HC08 processor.
Regards,

Alex

Message Edited by alex_spotw on 2006-07-28 12:28 PM

0 Kudos
Reply