differential measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

differential measurement

1,768 Views
juliancox
Contributor V

Is there any way to make a differential measurement using the A/D converter on any of the S08 devices? I am migrating an application from a '51 device where the A/D provides access to the Ain+ and Ain-. I am not sure if using 2 A/Ds and getting the difference in software will be reliable enough as it will probably double the error and I don't want to add a separate device.

Tags (2)
0 Kudos
Reply
2 Replies

1,610 Views
vicentegomez
NXP TechSupport
NXP TechSupport

You can use two adc channels 

Or you can use the analog comparator.


Just remember that the adc can not get negative inputs 

regards

Vicente 

0 Kudos
Reply

1,610 Views
juliancox
Contributor V

Using two channels is not a differential measurement - it is a post-conversion calculation. Each channel will be subject to the usual errors and therefore the potential error will be doubled. Also both inputs will be positive. With approximately 5000000 (sic) variants of the S08 I was really wondering if one of them had a differential input. If they could do it for the comparator, why not the A/D?

0 Kudos
Reply