development board list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

development board list

2,210件の閲覧回数
admin
Specialist II

Hello, I am not sure where the best place to post this question is, but does there exist an organized list of demo-boards made by Freescale or otherwise?  I get lost easily on the Freescale website, and I have a hard time finding what I am looking for.  I am experienced on the 9s12, but I would like to start playing with other controllers.  I would like to find an 8 or 16 bit demo-board where the target is through-hole and removable, so I can use it on a separate bread board for example.  So I guess I'm really looking for a programmer, maybe?  I noticed there are some programmers like I describe with 32 pin targets, but I would like no more than 20 pins.  Also I would like the target to have an internal oscillator.  Do these exist?  Thanks for your time.  I am sorry in advance if this is the wrong board.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,699件の閲覧回数
Encoder1
Contributor III

DEMO9S08QG8 seems in fact to fit your description: its uCU may be extracted from the Demoboard and equip an external breadboard. 9S08QG8 is a cheap 3.3V 16pin  low-end uCU.

Please consider that most Demoboards may also use their internal BDM port to program virgin or flashed uCU of the same series on external breadboard or PCB: this is quite the same than to use the uCU on the Demoboard, considered that the cost of this kind of device is 1 to 2$ for a new blank part.

I would chose DEMO9S08SH8 which can program either 9S08SH and -SQ part in the 20pin DIP inside or of any pinning size externally. This part is a 3.3-5V device and is more powerful and versatile than a 9S08QG8 and one of the few still available in the DIL size (20pin).

0 件の賞賛
返信

1,699件の閲覧回数
admin
Specialist II

I think this fits my description.

DEMO9S08QG8 Product Summary Page

Could I take this S08QG out of the demo board and use it with internal clock on a separate bread board?  Thanks.

0 件の賞賛
返信