a pager application with 1321xNSK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

a pager application with 1321xNSK

1,947件の閲覧回数
crafter
Contributor I
Hi Everybody,

I need assist on my zigbee project  "building a cluster tree messaging network". I thoght end devices will work as a pager. but here is the point should the SARD boards of 1321xNSK be an end device(reduced function device.) and should NCB be a Pan coordinator? or I should find any other product for end devices and set SARD boards for full function device. I m stuck at the beginning. What components do I have to use in this project. and what sources do you suggest me to look.   help of you guys will assist me to go deeper in zigbee world. thanks a lot.

serhat  
ラベル(1)
0 件の賞賛
返信
1 返信

1,055件の閲覧回数
NLFSJ
Contributor III
Hi,
 
Although I may not be able to reply to all your questions, the following information may be of assistance to you:
 
All of Freescale's development boards are programmable and capable of running as an end device (reduced function device) and a coordinator (full function device). 
 
The issue right now is that the ZigBee Stack (BeeStack) will not be released until February.  You can download the BeeKit from the Freescale website and use the 802.15.4 to setup a network
 
Regards,
Nina
0 件の賞賛
返信